Technical FAQs

Ask a Question

Which 800 series I/O modules are compatible with the Low Density 990QFC2005LD Quick Fit Conversion Connector?

The Quick Fit Conversion Connector makes for an easy migration to Quantum I/O. The below table contains a complete listing of Low Density 800 series I/O modules that are compatible with the 990QFC2005LD Conversion Connector.

Discrete Input
Discrete Output
B803-008
B802-008
B805-016
B804-116
B809-016
B804-148
B821-108
B808-016
B825-016
B810-008
B829-116
B814-108
B833-016
B820-008
B837-016
B824-016
B849-016
B828-016
B853-016
B832-016
B881-001
B840-108
text
B882-116
 
 

Legacy KB System (APS) Data: RESL170369 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?