Technical FAQs

Ask a Question

Are there 800 series I/O modules that cannot be used with the Quick Fit Conversion Connectors?

Yes. The 800 series I/O modules that are not compatible with the 990QFC2005LD and 990QFC2005HD Quick Fit Conversion Connectors are listed below:

800 I/O Not Compatible
B873-001
B873-011
B875-002
B875-012
B875-102
B882-239
B883-001
B883-101
B883-111
B883-200
B883-201
B884-002
B885-002
B885-100
B885-110
B984-100





 

Legacy KB System (APS) Data: RESL170368 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?