Technical FAQs

Ask a Question

Which 800 series I/O modules are compatible with the High Density 990QFC2005HD Quick Fit Conversion Connector?

The Quick Fit Conversion Connector makes for an easy migration to Quantum I/O. The below table contains a complete listing of High Density 800 series I/O modules that are compatible with the 990QFC2005HD Conversion Connector.

Discrete Input
Discrete Output
Analog I/O
B807-132
B806-032
B846-001
B817-116
B806-124
B846-002
B817-216
B826-032
B872-100
B827-032
B836-016
B872-200
B855-016
B838-032
B875-111
B863-032
B864-001
B875-200
B863-132
B881-108
B875-111
B865-001
B881-508
text
text
B882-032
text

Legacy KB System (APS) Data: RESL170367 V3.0, Originally authored by MiOB on 04/19/2011, Last Edited by MiOB on 04/19/2011
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?