Technical FAQs

Ask a Question

What is the maximum number of expansion modules that can be used with the TWDLCAE40DRF / TWDLCAA40DRF Twido controllers?

Up to 7 expansion modules can be used with the TWDLCAE40DRF / TWDLCAA40DRF controllers.


Legacy KB System (APS) Data: RESL170093 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon OTB
Was this helpful?
What can we do to improve the information ?