Technical FAQs

Ask a Question

Can I use a 140XCP90000 Battery Backup module to retain 3x count values on the Quantum high speed counters?

No, the Quantum 140EHC20200 and 140EHC10500 high speed counters cannot retain 3x register values with the
battery backup module during a power down. Counts can be moved to 4x holding registers if this information
must be stored.


Legacy KB System (APS) Data: RESL169825 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?