Technical FAQs

Ask a Question

How do you upgrade the firmware of the 140NWM100-00 FactoryCast HMI module?

Either the FCHMI software CD or your downloaded file will contain a folder named Add-ons. Click on this folder and then select the firmware folder. Select the folder for the Flash_NWM and inside that you will see two folders and two files. Open the upgradefw.exe application by double clicking. It shows an example of how you should enter the command line parameters. At the prompt enter the following:
<Module Type> <FTPFileName> <HostIP Address>

Command Line Example: NWM UpdateNWM.ftp

Was this helpful?
What can we do to improve the information ?