Technical FAQs

Ask a Question

How To Configure the XIP driver to use DNS

Goals and Symptoms

To explain how to configure the XIP driver for using DNS

Causes and Fixes


Click on the button named 'Configure XWAY IP Addresses'

  • Check off the DNS checkbox in the (Schneider Automation CNFXIP window) of the XIP driver.

  • Enter the 'Station Name' using hostname for the device or plc (i.e., na-achin3)
  • Enter an XWAY address (i.e., 4.1).
  • Click on the 'Add' button.

You can test the connection by clicking on 'Test\ICMP Ping'


Select the station from the dropdown list and click on the 'Ping' button.

Legacy KB System (APS) Data: RESL169687 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?