Technical FAQs

Ask a Question

Install error codes

Please see below the codes of the errors you could encounter installing Vijeo Look :
0 Success.
-1 General error.
-2 Invalid mode.
-3 Required data not found in the Setup.iss file.
-4 Not enough memory available.
-5 File does not exist.
-6 Cannot write to the response file.
-7 Unable to write to the log file.
-8 Invalid path to the InstallShield Silent response file.
-9 Not a valid list type (string or number).
-10 Data type is invalid.
-11 Unknown error during setup.
-12 Dialog boxes are out of order.
-51 Cannot create the specified folder.
-52 Cannot access the specified file or folder.
-53 Invalid option selected.


15/03/2005


Legacy KB System (APS) Data: RESL169554 V2.0, Originally authored by on , Last Edited by on
Related ranges: Vijeo Look
Was this helpful?
What can we do to improve the information ?