Technical FAQs

Ask a Question

What causes error 'E1072 variable expected' in Unity Pro?

This occurs on function blocks that use input/output parameters. It will be reported if the variable is assigned on the output of an INOUT pin rather than the input pin. It typically occurs on an import of a Concept project on an Analyze of the Unity Pro project.
Example:


Solution:
Move the variable from OUT to IN pin.


Legacy KB System (APS) Data: RESL169467 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?