Technical FAQs

Ask a Question

Is the ProWorx Plus v2.0 software available for installation by floppy disk format?

The ProWorx Plus v2.0 software only comes on a CD. However, there is a MAKEDISK utility on the ProWorx Plus v2.0 CD that allows you to transfer the software onto floppy disks for installation. You will need a total of 15 blank floppy disks to convert the ProWorx Plus v2.0 software from CD format. To access the MAKEDISK utility, open the Makedisk folder on the CD and launch the Makedisk.exe application. Follow the directions to install the ProWorx Plus v2.0 onto the 15 floppy disks.


Legacy KB System (APS) Data: RESL169449 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?