Technical FAQs

Ask a Question

What cable do you have to use for transferring application from PC to XBT H, P, E, terminal ?

Goals and Symptoms

 

What cable do you have to use for transferring application from PC to XBT terminal ?

Causes and Fixes

 

 
 
******************************************
If you use a serial port on your PC :
******************************************
For downloading application to a XBTG :
you have to use the XBTZG915 cable

For a XBT H-P-E-HM-PM-N401-NU400 :
you have to use the XBTZ915

For a XBT F :
you have to use the XBTZ915+XBTZ962

For a XBT N200/N400-R :
you have to use the XBTZ945


******************************************
If you use a USB port on your PC :
******************************************
For a XBTG :
you have to use the XBTZG925

For a XBT H-P-E-HM-PM-N401-NU400 :
you can use the SR2CBL06 (1) + XBTZ915

(see attached file "usb cable to transfer appli")

For a XBT F :
you can use the SR2CBL06 (1) + XBTZ915+XBTZ962
(see attached file)

For a XBT N200/N400-R :
you can use the SR2CBL06 (1) + XBTZ945
(see attached file)

(1) CAUTION:
This cable is qualified for XBT N/R
This cable is not qualified for XBT H/P/E,/HM/PM/F, it could works as workaround (it is not supported)

For more information, please refer to the "Automation and Control, HUMAN_MACHINE_INTERFACEs" catalog.

Attachments

(Removed File URL: 169306_80EE/SR2CBL06_usb_cable_to_transfer_appli_XBTN-R.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/c389e8c42461abedc1257209005278b3/fl_block_5/0.1406?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL169306 V4.0, Originally authored by on , Last Edited by FaMe on 10/16/2006
Related ranges: Magelis XBT H, XBT P, XBT E
Was this helpful?
What can we do to improve the information ?