Technical FAQs

Ask a Question

How can I add help files to DFBs that I write in Unity Pro?

Unity Pro provides a function called "Add Hyperlink". Right click on a DFB, section, or anything in the Project navigation list.
Assign a name and then point to a path that contains a file. This can be a .doc, .txt, .pdf, etc.file and should contain your Help instructions.
You will then see it under the DFB, for example, as a small blue ball. Clicking on this brings up the Help screen that you have created.


Legacy KB System (APS) Data: RESL169298 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?