Technical FAQs

Ask a Question

How to transfer the Vijeo Look V2.5 licence if the Entry Code of the target computer is "0" ?

Goals and Symptoms

How to transfer the Vijeo Look V2.5 licence if the Entry Code of the target computer is "0" ?
 

Causes and Fixes

An Entry Code equal to 0 isn't valid.

So please follow the below procedure to get a valid Entry Code of the target PC :
1- Install VJL V2.5 on the target PC.
2- Restart your target PC.
3- Enter Vijeo Look program by using "Start/Programs/Schneider electric/Vijeo Look/Vijeo Look"
4- You get a message saying "this product is not yet licenced". Click on the "Register" button.
5- Click on "Next"
6- You get a message saying "Select task".
Don't click on "Transfer authorisation", you would get an Entry Code = 0.
But click on "Enter received code". You will then get your Computer ID and your Code Entry Number.
7- With these numbers, all should work.


Legacy KB System (APS) Data: RESL169245 V1.0, Originally authored by on , Last Edited by on
Related ranges: Vijeo Look
Was this helpful?
What can we do to improve the information ?