Technical FAQs

Ask a Question

Can you transfer ProWORX NxT traffic cop data from one database to other databases?

Yes, you can transfer ProWorx NxT traffic cop data from one database to other databases. This can be done through the NxT Import/Export utility. To access the utility go to "File", "Utilities", "Import/Export".


Legacy KB System (APS) Data: RESL168976 V2.0, Originally authored by PeZa on 11/22/2012, Last Edited by RoAl on 11/22/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?