Technical FAQs

Ask a Question

Can I edit user logic when using the ProWORX 32 emulator?

 

The emulation function in ProWORX 32 is used to test the integrity of the logic in a project without the need of a PLC. Emulation mode allows you to check discrete states and register contents, and test your logic. You cannot edit user logic in emulaton mode.

Legacy KB System (APS) Data: RESL168877 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?