Technical FAQs

Ask a Question

Can I use the ProWORX 32 Compare utility to do a compare of two databases with the same project name?

ProWORX 32 software only allows the *.PWX files to be accessed from the Projects folder, so the databases cannot have the same name. You would need to save/rename one of the ProWORX 32 database projects with a different name to successfully run the compare.

Legacy KB System (APS) Data: RESL168544 V2.0, Originally authored by PeZa on 12/07/2012, Last Edited by RoAl on 12/07/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?