Technical FAQs

Ask a Question

How do I get ProWorx NxT to open the Instruction Edit window when adding a new instruction in logic instead of the cursor jumping to the right of the instruction?

This is simply an issue with the NxT Preferences setting and can be corrected by checking off the option for "Display Editor for New Instructions" in the NxT Preferences window. Once this option is checked off, the cursor will stop jumping to the right of the instruction and open the Instruction Edit window immediately.


Legacy KB System (APS) Data: RESL168531 V2.0, Originally authored by PeZa on 12/07/2012, Last Edited by RoAl on 12/07/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?