Technical FAQs

Ask a Question

Unity SFCVIEW: restriction for name conventions

Goals and Symptoms

1. SFC View accepts only Alias names, which contain at least one letter.
OFS and DLAG view are working with pure numerical Alias names.

2. Unity SFC View does not accept, if in two paths of the functional view the same struktur is used.

Facts and Changes

Unity SFCVIEW V2.0: UNYSDUMFUCD20

Causes and Fixes

Do not use Alias Names without letters.
Do not use in two paths of the functional view the same structure.
Problems are solved in Unity SFC View V2.0 patch a.

Was this helpful?
What can we do to improve the information ?