Technical FAQs

Ask a Question

Does the Concept 2.6 Application Loader, 372SPU47701, allow importing of an .ASC file?

The Concept Application Loader (372 SPU 477 01 V26. ) does allow the importing of .ASC files through the Concept Converter. It also allows the user to open a .prz (archived) project. The execloader is also included.


Legacy KB System (APS) Data: RESL168357 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?