Technical FAQs

Ask a Question

How do I configure a double slot power supply in a Premium rack within the hardware configuration screen of PL7 software?

PL7 inserts the Processor into Slot 0 and a single wide power supply when a new application is created. To insert a double slot power supply, move the processor from slot 0 to slot 1. Double click on the existing power supply. You can now select one of the double slot power supply in the list.


Legacy KB System (APS) Data: RESL168157 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?