Technical FAQs

Ask a Question

How can I force a value in a 3x register while online with the PLC using Concept?

No. A 3x register can not have a value forced into it via the RDE while online with the PLC. In Concept, you will see that the value of the 3x register is grayed out and does not accept values written into it. The 3x register is an input register which is mapped to I/O. This allows field data to be brought into the PLC application.


Legacy KB System (APS) Data: RESL168087 V2.0, Originally authored by RiVe on 05/02/2013, Last Edited by DiSa on 05/02/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?