Technical FAQs

Ask a Question

Is it possible in PL7 to edit a DFB that is in use in the application?

No, it is not possible.You must first delete any instance of the DFB in the application before you can edit the DFB.


Legacy KB System (APS) Data: RESL168081 V1.0, Originally authored by on , Last Edited by on
Related ranges: PL7
Was this helpful?
What can we do to improve the information ?