Technical FAQs

Ask a Question

Converting a ProWORX NxT application that has a Profibus configuration extension defined.

Goals and Symptoms

Converting a ProWORX NxT application that has a Profibus configuration extension defined.

Facts and Changes

Convertion Modsoft - Concept

Causes and Fixes

Use the following procedure to convert a ProWORX NxT application that has "Profibus configured to a Concept project.

1.) Download the NxT project to the plc.
2.) Upload the plc application using Concept.
3.) Save the project.
4.) Check the configuration extension to ensure that the Profibus option is checked off.
5.) Check the IO Map to see if the 140 CRP 811 module is in the configuration.
6.) Click on the Params button in the IO Map to bring up the Profibus information for the CRP 811 module.
7.) Click on the button Add Upload Info.
8.) Click on the OK button
9.) Repeat steps 6 through 8 for each configured 140 CRP 811 module.
9.) Save the changes.
10.) Upload the plc application again.


Legacy KB System (APS) Data: RESL168029 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modsoft
Was this helpful?
What can we do to improve the information ?