Technical FAQs

Ask a Question

Nxt returns 'Overflow = 006' error message when trying to print the visual traffic cop.

Goals and Symptoms

Nxt returns 'Overflow = 006' error message when trying to print the visual traffic cop.

Facts and Changes

If the description is too long and there is no carriage return detected, the error will get returned.

Causes and Fixes

To resolve this problem, check the descritption to see if a carriage return is used after each line of the description or shorten the description.


Legacy KB System (APS) Data: RESL167880 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?