Technical FAQs

Ask a Question

Use of 174CEV30020 with 984B controller

Goals and Symptoms

An issue has been found with the combination of a 174CEV30020 V1.3 Modbus/Ethernet gateway and a 984B controller connected over RS-232 at 19,200 baud .

Facts and Changes

The 984B worked fine with the 174CEV30010 at 19,200 baud and it works fine at 9,600 baud with the 174CEV30020

Causes and Fixes

Since this problem only seems to happen with this combination and this is a new exec that solved similar issues in many other environments there is no planned change to address this issue. Therefore we do not recommend using 174CEV20030 and 984B controllers at 19,200 baud.


Legacy KB System (APS) Data: RESL167769 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?