Technical FAQs

Ask a Question

What causes a runtime error -21478105' in ProWORX 32?

This runtime error can usually be fixed by installing SP3 for the Jet Drivers 4.0 which is used with ProWORX 32. This patch can be found on the installation CD in the \MDAC\folder.


Legacy KB System (APS) Data: RESL167657 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?