Technical FAQs

Ask a Question

Using OFS in DCOM architecture after installing Windows XP SP2


In order to use OFS with DCOM clients after installing Windows XP SP2 you must desable FIREWALL
If you wish better tunning concerning security on the PC the follwing link can help you

 

List of Com+ fixes in Windows XP Service Pack 2
http://support.microsoft.com/default.aspx?scid=kb;en-us;838211

DCOM Security Enhancements
http://msdn.microsoft.com/security/productinfo/XPSP2/networkprotection/dcom.aspx

Connecting Through Windows Firewall
http://msdn.microsoft.com/library/default.asp?url=/library/en-us/wmisdk/wmi/connecting_through_windows_firewall.asp

Legacy KB System (APS) Data: RESL167319 V1.0, Originally authored by on , Last Edited by on
Related ranges: OFS
Was this helpful?
What can we do to improve the information ?