Technical FAQs

Ask a Question

What are the DIN rail dimensions for an Advantys island?

The DIN rail is 35 mm (1.38 in) high. There are two depth sizes of DIN rail you can use with an Advantys island, 7.5 mm (0.3 in) and 15 mm (0.6 in).


Legacy KB System (APS) Data: RESL167265 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys Telefast ABE 7
Was this helpful?
What can we do to improve the information ?