Technical FAQs

Ask a Question

What are the physical dimensions for the STBXMP4440 removable memory card?

The STBXMP4440 removable memory card measures 25.1 mm (0.99 in) wide x 15 mm (0.59 in) high x 0.76 mm (0.30 in) thick. It is shipped as a punch-out on a credit-card-sized plastic card, which measures 85.6 mm (3.37 in) wide x 53.98 mm (2.13 in) high.

Was this helpful?
What can we do to improve the information ?