Technical FAQs

Ask a Question

Can programs created with ProWORX NxT be opened with the ProWORX 32 software?

Yes. Programs created with ProWORX NxT can be imported, then opened, using ProWORX 32 software. With the ProWORX 32 software up and running, go to <FILE> then <IMPORT DATABASE>, select File Type as (*.DCF) for ProWORX NxT, then go into the folder that has the NxT *.DCF file and select it, click on the <OPEN> button and the conversion process will begin.


Legacy KB System (APS) Data: RESL167256 V2.0, Originally authored by PeZa on 07/18/2013, Last Edited by RoAl on 07/18/2013
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?