Technical FAQs

Ask a Question

Can I use both ports A and B simultaneously on the B885-002 module?

No, both ports A and B on the B885-002 module cannot be used simultaneously. Only one port can be running at any given time. The B885-002 module has a slide switch for either RUN or PROGRAM. If the slide switch is set to PROGRAM, then one port has to be used for the programming device. If the slide switch is set to RUN, then both ports can be used for field devices.


Legacy KB System (APS) Data: RESL167255 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?