Technical FAQs

Ask a Question

How do I terminate my repeater on a MB+ network?

The image below shows an RR85 in different topological hardware configurations with proper termination.
The general rule is if the repeater is at the end of the trunk it will require termination and if in the middle of the trunk will have an in-line connector.
However if the repeater is a 490NRP253, fiber repeater, there would obviously be no termination on the fiber side.

Was this helpful?
What can we do to improve the information ?