Technical FAQs

Ask a Question

What are the valid FIPIO node address settings for the Advantys STBNFP2212?

The valid FIPIO address settings for the Advantys STBNFP2212 are 1-127, excluding address 63. FIPIO reserves address 0 for the FIPIO master and address 63 for programming and diagnostics. While it is possible to physically set the rotary address switches on the NIM to either of these addresses, they should not be used for proper operation.

Was this helpful?
What can we do to improve the information ?