Technical FAQs

Ask a Question

Does the Redundancy Manager switch need to be set on all of the Connexium Ethernet switches in a fiber optic ring, or is it set on only one of them?

The Redundancy Manager switch should only be set on one Connexium switch in a fiber optic ring. all other Connexium switches on that ring should have the Redundancy Manager switch turned off.


Legacy KB System (APS) Data: RESL167151 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?