Technical FAQs

Ask a Question

What causes a 'write error to file - (write protected) Error Id - 1323' when opening a Concept project?

This error is displayed if the attributes of the files within the project are set to 'read only'. Open the Windows Explorer, highlight the project files, right click and open 'Properties' and uncheck the 'read only' box.


Legacy KB System (APS) Data: RESL167054 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?