Technical FAQs

Ask a Question

Can I export an IL section and import it as an FBD section?

Yes, export the section as IEC text. (File - Export -IEC text. ) Assign the output file a .txt extension.
Open your existing or new project and go to File - import IEC text with FBD option.
If you get an error, double click on the error and delete it from the file. Close the file with the 'x' in the upper right corner.
File - import IEC text again and it should import without any errors and create the FBD section.


Legacy KB System (APS) Data: RESL166976 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?