Technical FAQs

Ask a Question

What is the difference between the Compact AS-BADU-206 and the AS-BADU-256 analog input modules?

The only difference between the two Compact analog input modules is that the AS-BADU-256 module operates at extended temperatures.
Operating Temperature:
AS-BADU-206.....0 to +60 degrees C
AS-BADU-256.....-40 to +70 degrees C


Legacy KB System (APS) Data: RESL166975 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?