Technical FAQs

Ask a Question

How do you enter 'Related Documents' in the ProWORX 32 Server?

The user can add or delete documents that can be accessed through the ProWORX 32 Server. Move the document to \Proworx\32\Server\Related Documents. These documents can be viewed in the Proworx 32 server by going to the 'Related Documents' tab and double clicking on the document. ProWORX 32 Server will bring up the file's specified editor.
Right clicking on the navigation tree will allow the user to add, remove, get, put and unlock the documents.


Legacy KB System (APS) Data: RESL166721 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?