Technical FAQs

Ask a Question

What causes error message "autoexec.nt could not be used to use MSDOS and windows apps" when trying to launch Concept?

One possible reason is that the autoexec.nt file is not in the windows\system32 folder. It may be in another folder. Moving it to the \windows\system32 folder should correct this.

Was this helpful?
What can we do to improve the information ?