Technical FAQs

Ask a Question

What is the part number for the Advantys marking label sheets?

The part number for the Advantys marking label sheets is STBXMP6700 and they are sold in lots of twenty five. Each individual I/O base and module combination has two spaces on its front reserved for marking labels. Using marking labels can help you quickly identify information on individual bases and modules. They can also help match I/O to their matching bases.


Legacy KB System (APS) Data: RESL165478 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?