Technical FAQs

Ask a Question

Is there a setting that will devote the entire screen to the Logic Editor in ProWORX 32?

Go to <Properties><Environment> <Environment> and check 'Enable Scrolling Navigation Panel'. When a project's Logic Editor is open, the logic screen will fill the width of the screen. Dragging the mouse to the far left of the screen brings back the Navigation Panel.


Legacy KB System (APS) Data: RESL165097 V1.0, Originally authored by on , Last Edited by on
Related ranges: Domino
Was this helpful?
What can we do to improve the information ?