Technical FAQs

Ask a Question

Does Schneider Electric offer an external monitor for the Magelis iPC ?

Yes. There are 4 external LCD monitors available for the Magelis iPC. The monitors attach to the VGA port on the control box.
Part # information is provided below.
 

Part #
Screen Size
Power Requirement
MPC YS2 0NAN 00N
12"
115-230 VAC 50/60 Hz
MPC YS2 0NDN 00N
12"
24 VDC
MPC YS5 0NAN 00N
15"
115-230 VAC 50/60 Hz
MPC YS5 0NDN 00N
15"
24 VDC

Legacy KB System (APS) Data: RESL164857 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis Modular iPC
Was this helpful?
What can we do to improve the information ?