Technical FAQs

Ask a Question

Why is the "OK" button grayed out in the ProWorx 32 Communications Setup window?

The "OK" button will be grayed out in the Communication Setup window when you're in MONITOR mode. Once you switch over to PROGRAM mode, the "OK" button will be activated.


Legacy KB System (APS) Data: RESL164808 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?