Technical FAQs

Ask a Question

Does the TSX Compact CPU module have to be mounted in the left most slot of a AS-HDTA-200 rack?

Yes. The TSX Compact CPU module must always be installed in th left-most slot of the AS-HDTA-200 rack. It is not compatible with any other model rack or slot number.


Legacy KB System (APS) Data: RESL164799 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?