Technical FAQs

Ask a Question

What replaces the AS-BSIM-203?

There is unfortunately no replacement for the AS-BSIM-203 offered. The user would need to use a set of potentiometers, a voltmeter and appropriate field wiring for the Analog I/O modules being utilized to perform the same function.


Legacy KB System (APS) Data: RESL164797 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?