Technical FAQs

Ask a Question

Use of Phoenix Ethernet IO FB IL 24 BK Modules

Goals and Symptoms

This resolution describes the use of Phoenix Ethernet IO modules in a network mixed with Quantum and Momentum Ethernet devices.

Facts and Changes

The Phoenix FL IL24 BK ethernet I/O module was setup using the Phoenix Factory line IO configuration software. The module is similar in style as ourr Advantys modules. The module has a watchdog timer setup that stops the module if it loses communication for more the the set value. In this application it was 10 seconds. The module then has to be restarted before you can communicate with it again.

Causes and Fixes

In our testing we found that the module worked in our test environment and seemed to respond without any issues.


Legacy KB System (APS) Data: RESL164752 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum NOE - TR
Was this helpful?
What can we do to improve the information ?