Technical FAQs

Ask a Question

Will the extended memory (6X registers) be saved during a power failure?

The extended memory (6X register) values are stored in state ram. These values will be saved during a power failure as long as a backup battery is installed, and the battery is good.


Legacy KB System (APS) Data: RESL164524 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?