Technical FAQs

Ask a Question

Is the Compact Interbus S Master 'AS-BBKF-201' a 16 word or 64 word module?

The Compact Interbus S Master Module "AS-BBKF-201" can be setup for either 16 or 64 word. It all depends on what you setup the Dip switch settings for S0 and S1. The Dip switch configuration settings for S0 and S1 are explained in Chapter 11 from the latest Modicon A120 Series I/O Modules User Guide (890USE10900 Version 4.0).

Was this helpful?
What can we do to improve the information ?