Technical FAQs

Ask a Question

Is there a means in ProWorx NxT to display the amount of logic used in a PLC program?

Yes. While on-line with the controller click on "Display", and then select "logic used" from the pull down. This will show how much is used out of what is available in the controller. This feature is only available while on-line with a controller. There is no means to view this while in off-line mode.


Legacy KB System (APS) Data: RESL164462 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?