Technical FAQs

Ask a Question

Why does my 140ACI03000 map to 9 input registers when it only has 8 input channels?

140ACI03000 requires 9 words of addressing. The 9'th word is a status register used for over range/ broken wire indication.

 
Was this helpful?
What can we do to improve the information ?